NXP Reader Library  v17.1.0.2535
phCryptoSym_Sw_DataParams_t Struct Reference

Data structure for Symmetric Crypto Software layer implementation. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
uint8_t bLrpEnabled
 This specifies whether LRP Mode is enabled or not.
 
uint8_t bNumofKeystoUpdate
 This specifies the Number of times the Key to be updated while generating the SPT.UpdatedKey.
 
uint32_t dwEncCtr
 This specifies the counter maintained which to increment for every Encryption/Decryption.
 
void * pKeyStoreDataParams
 Pointer to Key Store object - can be NULL.
 
uint8_t pKey [PH_CRYPTOSYM_SW_KEY_BUFFER_SIZE *16]
 Internal key storage array.
 
uint8_t pIV [PH_CRYPTOSYM_SW_MAX_BLOCK_SIZE]
 Internal IV storage array.
 
uint16_t wKeyType
 Key Type.
 
uint16_t wKeepIV
 Indicates if the init vector of a previous crypto operation shall be used for the next operation.
 
uint16_t wAddInfo
 Additional information like diversified key length, etc.
 

Detailed Description

Data structure for Symmetric Crypto Software layer implementation.


The documentation for this struct was generated from the following file: