NXP Reader Library  v17.1.0.2535
phKeyStore_Rc663_DataParams_t Struct Reference

Rc663 parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
void * pHalDataParams
 Pointer to the parameter structure of the underlying layer.
 

Detailed Description

Rc663 parameter structure.


The documentation for this struct was generated from the following file: