NXP Reader Library  v17.1.0.2535
phKeyStore_SamAV3_KeyEntry_t Struct Reference

SamAV3 Key Entry Structure. More...

Data Fields

uint8_t aKeyData [48]
 Concatenated KeyA, KeyB, KeyC (used only for ChangeKeyEntry, cleared by GetKeyEntry).
 
uint8_t aDFAid [3]
 DESfire AID.
 
uint8_t bDFKeyNo
 Corresponding DESFire key number (of DESFire AID).
 
uint8_t bKeyNoCEK
 Key reference number of change entry key.
 
uint8_t bKeyVCEK
 Key version of change entry key.
 
uint8_t bRefNoKUC
 Reference number of key usage counter.
 
uint8_t bKeyNoAEK
 Key reference number of Access Key Entry.
 
uint8_t bKeyVAEK
 Key reference version of Access Key Entry.
 
uint8_t aSet [2]
 Configuration settings of this key entry.
 
uint8_t bVersionKeyA
 Version of Key A.
 
uint8_t bVersionKeyB
 Version of Key B.
 
uint8_t bVersionKeyC
 Version of Key C.
 
uint8_t aExtSet [2]
 Extended configuration settings of this key entry.
 
uint8_t bVersionKeyBValid
 Indicates whether Key B Version is available or not.
 
uint8_t bVersionKeyCValid
 Indicates whether Key C Version is available or not.
 

Detailed Description

SamAV3 Key Entry Structure.


The documentation for this struct was generated from the following file: