NXP Reader Library  v17.1.0.2535
phKeyStore_Sw_KeyEntry_t Struct Reference

Software KeyEntry structure. More...

Data Fields

uint16_t wKeyType
 Type of the keys in Key-Version Pair.
 
uint16_t wRefNoKUC
 Key usage counter number of the keys in pKeys.
 

Detailed Description

Software KeyEntry structure.


The documentation for this struct was generated from the following file: