NXP Reader Library  v17.1.0.2535
phTMIUtils_t Struct Reference

Definition of a singe Log entry. More...

Data Fields

uint8_tpTMIBuffer
 Pointer to TMI Buffer.
 
uint32_t dwTMIBufLen
 Length of TMI Buffer.
 
uint32_t dwTMIbufIndex
 Pointer indicating the TMI Buffer fill index.
 
uint8_t bTMIStatus
 Indicates whether TMI collection is PH_ON or PH_OFF.
 
uint32_t dwOffsetInTMI
 Indicates the offset in TMI buffer where the Length field is stored in case of unspecified length read.
 

Detailed Description

Definition of a singe Log entry.


The documentation for this struct was generated from the following file: