Data structure for MIFARE DUOX Software layer implementation
More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pPalMifareDataParams |
| Pointer to the parameter structure of the palMifare component. | |
| void * | pKeyStoreDataParams |
| Pointer to the parameter structure of the KeyStore layer. | |
| void * | pCryptoDataParamsASym |
| Pointer to the parameter structure of the ASymmetric Crypto component. | |
| void * | pCryptoDataParamsEnc |
| Pointer to the parameter structure of the Symmetric Crypto layer for encryption. | |
| void * | pCryptoDataParamsMac |
| Pointer to the parameter structure of the Symmetric Crypto layer for MACing. | |
| void * | pCryptoRngDataParams |
| Pointer to the parameter structure of the Crypto layer for Random number generation. | |
| void * | pTMIDataParams |
| Pointer to the parameter structure for collecting TMI. | |
| void * | pVCADataParams |
| Pointer to the parameter structure for Virtual Card. | |
| uint8_t * | pCmdBuf |
| Pointer to global buffer for processing the command. | |
| uint16_t | wCmdBufSize |
| Size of global command buffer. | |
| uint16_t | wCmdBufLen |
| Length of bytes available in command buffer (pCmdBuf) for processing. | |
| uint16_t | wCmdBufOffset |
| Command Buffer offset while performing crypto or exchange operations. | |
| uint8_t * | pPrsBuf |
| Pointer to global buffer for processing the response / secure messaging information. | |
| uint16_t | wPrsBufSize |
| Size of global response / secure messaging information buffer. | |
| uint16_t | wPrsBufLen |
| Length of bytes available in response / secure messaging information buffer (pPrsBuf) for processing. | |
| uint16_t | wPrsBufOffset |
| Processing Buffer offset while performing crypto or exchange operations. | |
| uint8_t | aAid [3] |
| Aid of the currently selected application. | |
| uint8_t | aSesAuthENCKey [PH_CRYPTOSYM_AES128_KEY_SIZE *2] |
| Authentication Encryption key for the session. | |
| uint8_t | aSesAuthMACKey [PH_CRYPTOSYM_AES128_KEY_SIZE *2] |
| Authentication MAC key for the session. | |
| uint8_t | aTi [PHAL_MFDUOX_SIZE_TI] |
| Transaction Identifier of the current transaction. | |
| uint16_t | wCmdCtr |
| Command count within transaction. | |
| uint16_t | wAdditionalInfo |
| Specific error codes for MIFARE DUOX generic errors or To get the response length of some commands. | |
| uint8_t | bWrappedMode |
| Wrapped APDU mode. More... | |
| uint8_t | bShortLenApdu |
| One of the following,. More... | |
| uint8_t | bCmdCode |
| Command code. More... | |
| uint8_t | bAuthState |
| Authenticate Command used. More... | |
| uint8_t | bKeyNo |
| Key number against which this authentication is done. | |
| uint16_t | wKeyType |
| Key Type being used for Authentication. | |
| uint8_t | bPICCDataComplete |
| Flag to Indicate PICC data Status. More... | |
| uint8_t | bHasMACProcessed |
| Flag to indicate if MAC verification is complete for response or MAC computation is complete for Command. More... | |
| uint8_t | bIsENCPending |
| Flag to indicate if Encryption of Data is complete or still pending. | |
Data structure for MIFARE DUOX Software layer implementation
| uint8_t phalMfDuoX_Sw_DataParams_t::bWrappedMode |
Wrapped APDU mode.
All native commands need to be sent wrapped in ISO 7816 APDUs.
| uint8_t phalMfDuoX_Sw_DataParams_t::bShortLenApdu |
One of the following,.
| uint8_t phalMfDuoX_Sw_DataParams_t::bCmdCode |
Command code.
This will be used for differentiating the same error codes for different commands.
| uint8_t phalMfDuoX_Sw_DataParams_t::bAuthState |
Authenticate Command used.
One of the below values will be updated
| uint8_t phalMfDuoX_Sw_DataParams_t::bPICCDataComplete |
Flag to Indicate PICC data Status.
Indicates the following.
| uint8_t phalMfDuoX_Sw_DataParams_t::bHasMACProcessed |
Flag to indicate if MAC verification is complete for response or MAC computation is complete for Command.
This flag will also be used to indicate the status of initial MAC processing.