MIFARE PRIME NTAG SAM AV3 NonX parameter structure
More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| phhalHw_SamAV3_DataParams_t * | pHalSamDataParams |
| Pointer to the parameter structure of the hal of the SAM layer. | |
| void * | pPalMifareDataParams |
| Pointer to the parameter structure of the palMifare component. | |
| uint8_t | bAuthMode |
| Auth. More... | |
| uint8_t | bKeyNo |
| Key number against which authenticated. | |
| uint8_t | aAid [3] |
| Currently selected application Id. | |
| uint16_t | wAdditionalInfo |
| Specific error codes for Desfire generic errors or error codes returned by the card. | |
MIFARE PRIME NTAG SAM AV3 NonX parameter structure
| uint8_t phalMfPrimeNtag_SamAV3_NonX_DataParams_t::bAuthMode |
Auth.
Mode 0x0A or Ox1A or OxAA.