NXP Reader Library  v17.1.0.2535
phalMfPrimeNtag_SamAV3_X_DataParams_t Struct Reference

MIFARE MIFARE PRIME NTAG SAM AV3 X parameter structure
More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_SamAV3_DataParams_tpHalSamDataParams
 Pointer to the parameter structure of the hal of the SAM layer.
 
uint8_t bAuthMode
 Auth Mode. More...
 
uint8_t bKeyNo
 Key number against which authenticated.
 
uint8_t aAid [3]
 Currently selected application Id.
 
uint16_t wAdditionalInfo
 Specific error codes for Desfire generic errors or error codes returned by the card.
 

Detailed Description

MIFARE MIFARE PRIME NTAG SAM AV3 X parameter structure

Field Documentation

◆ bAuthMode

uint8_t phalMfPrimeNtag_SamAV3_X_DataParams_t::bAuthMode

Auth Mode.

0x0A or 0x1A or 0xAA.


The documentation for this struct was generated from the following file: