NXP Reader Library  v17.1.0.2535
phalMfc_SamAV2_X_DataParams_t Struct Reference

SamAV2 AL-MFC parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_SamAV2_DataParams_tpHalDataParams
 Pointer to the parameter structure of the underlying HAL layer.
 
phpalMifare_SamAV2_X_DataParams_tpPalMifareDataParams
 Pointer to the parameter structure of the palMifare component.
 

Detailed Description

SamAV2 AL-MFC parameter structure.


The documentation for this struct was generated from the following file: