NXP Reader Library  v17.1.0.2535
phalMfc_SamAV3_X_DataParams_t Struct Reference

SamAV3 AL-MFC parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_SamAV3_DataParams_tpHalDataParams
 Pointer to the parameter structure of the underlying HAL layer.
 
void * pPalMifareDataParams
 Pointer to the parameter structure of the palMifare component.
 

Detailed Description

SamAV3 AL-MFC parameter structure.


The documentation for this struct was generated from the following file: