NXP Reader Library  v17.1.0.2535
phalMfc_Sw_DataParams_t Struct Reference

Private parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
void * pPalMifareDataParams
 Pointer to the parameter structure of the palMifare component.
 
void * pKeyStoreDataParams
 Pointer to the parameter structure of the KeyStore component.
 

Detailed Description

Private parameter structure.


The documentation for this struct was generated from the following file: