MIFARE DESFire EVx SAM NonX parameter structure
More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| phhalHw_SamAV3_DataParams_t * | pHalSamDataParams |
| Pointer to the parameter structure of the HAL of the SAM layer. | |
| void * | pPalMifareDataParams |
| Pointer to the parameter structure of the palMifare component. | |
| phTMIUtils_t * | pTMIDataParams |
| Pointer to the parameter structure for collecting TMI. | |
| uint8_t * | pTmpBuffer |
| Temporary buffer for framing the command buffer. | |
| uint16_t | wTmpBufSize |
| Size of Temporary buffer. | |
| uint8_t | bAuthMode |
| Authentication. More... | |
| uint8_t | bKeyNo |
| Key number against which authenticated. | |
| uint8_t | bWrappedMode |
| Wrapped APDU mode. More... | |
| uint8_t | bExtendedLenApdu |
| Extended length APDU. More... | |
| uint8_t | pAid [3] |
| Currently selected application Id. | |
| uint16_t | wAdditionalInfo |
| Specific error codes for DESFire generic errors or error codes returned by the card. | |
| uint8_t | bCmdCode |
| Command code. More... | |
| uint8_t | bUid [15] |
| Complete UID of the PICC. More... | |
| uint8_t | bUidLength |
| Length of bytes available in bUid buffer. | |
| uint8_t | bReturn_FabID |
| Get / Set the return of Fabrication Identifier. More... | |
MIFARE DESFire EVx SAM NonX parameter structure
| uint8_t phalMfdfEVx_SamAV3_NonX_DataParams_t::bAuthMode |
Authentication.
Mode 0x0A or Ox1A or OxAA.
| uint8_t phalMfdfEVx_SamAV3_NonX_DataParams_t::bWrappedMode |
Wrapped APDU mode.
All native commands need to be sent wrapped in ISO 7816 APDU's
| uint8_t phalMfdfEVx_SamAV3_NonX_DataParams_t::bExtendedLenApdu |
Extended length APDU.
If set the native commands should be wrapped in extended format
| uint8_t phalMfdfEVx_SamAV3_NonX_DataParams_t::bCmdCode |
Command code.
This will be used for differentiating the common error codes between different commands.
| uint8_t phalMfdfEVx_SamAV3_NonX_DataParams_t::bUid[15] |
Complete UID of the PICC.
This will be updated when phalMfdfEVx_GetCardUID interface is called.
| uint8_t phalMfdfEVx_SamAV3_NonX_DataParams_t::bReturn_FabID |
Get / Set the return of Fabrication Identifier.
When Set will be utilized during GetVersion command exchange.