NXP Reader Library  v17.1.0.2535
phalMfdfEVx_Sw_DataParams_t Struct Reference

Data structure for MIFARE DESFire EVx Software layer implementation
More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
void * pPalMifareDataParams
 Pointer to the parameter structure of the palMifare component.
 
void * pKeyStoreDataParams
 Pointer to the parameter structure of the KeyStore layer.
 
void * pCryptoDataParamsEnc
 Pointer to the parameter structure of the Crypto layer for encryption.
 
void * pCryptoDataParamsMac
 Pointer to the parameter structure of the CryptoMAC.
 
void * pCryptoRngDataParams
 Pointer to the parameter structure of the CryptoRng layer.
 
void * pHalDataParams
 Pointer to the HAL parameters structure.
 
uint8_t bSesAuthENCKey [24]
 Session key for this authentication.
 
uint8_t bKeyNo
 Key number against which this authentication is done.
 
uint8_t bIv [16]
 Max size of IV can be 16 bytes.
 
uint8_t bAuthMode
 Authenticate (0x0A), AuthISO (0x1A), AuthAES (0xAA)
 
uint8_t bCmdCode
 Command code. More...
 
uint8_t pAid [3]
 Aid of the currently selected application.
 
uint8_t bCryptoMethod
 DES,3DES, 3K3DES or AES.
 
uint8_t bWrappedMode
 Wrapped APDU mode. More...
 
uint16_t wCrc
 2 Byte CRC initial value in Authenticate mode.
 
uint32_t dwCrc
 4 Byte CRC initial value in 0x1A, 0xAA mode.
 
uint16_t wAdditionalInfo
 Specific error codes for DESFire generic errors or To get the response length of some commands.
 
uint32_t dwPayLoadLen
 Amount of data to be read. More...
 
uint16_t wCmdCtr
 Command count within transaction.
 
uint8_t bTi [PHAL_MFDFEVX_SIZE_TI]
 Transaction Identifier.
 
uint8_t bSesAuthMACKey [16]
 Authentication MAC key for the session.
 
uint8_t pUnprocByteBuff [PHAL_MFDFEVX_SIZE_MAC]
 Buffer containing unprocessed bytes for read mac answer stream.
 
uint8_t bNoUnprocBytes
 Amount of data in the pUnprocByteBuff.
 
uint8_t bLastBlockBuffer [16]
 Buffer to store last Block of encrypted data in case of chaining.
 
uint8_t bLastBlockIndex
 Last Block Buffer Index.
 
void * pTMIDataParams
 Pointer to the parameter structure for collecting TMI.
 
uint8_t bShortLenApdu
 Parameter for force set Short Length APDU in case of BIG ISO read.
 
void * pVCADataParams
 Pointer to the parameter structure for Virtual Card.
 
uint8_t bUid [15]
 Complete UID of the PICC. More...
 
uint8_t bUidLength
 Length of bytes available in bUid buffer.
 
uint8_t bSDMStatus
 Get / Set the SDM availability in the file.
 
uint8_t bReturn_FabID
 Get / Set the return of Fabrication Identifier. More...
 

Detailed Description

Data structure for MIFARE DESFire EVx Software layer implementation

Field Documentation

◆ bCmdCode

uint8_t phalMfdfEVx_Sw_DataParams_t::bCmdCode

Command code.

This will be used for differentiating the common error codes between different commands.

◆ bWrappedMode

uint8_t phalMfdfEVx_Sw_DataParams_t::bWrappedMode

Wrapped APDU mode.

All native commands need to be sent wrapped in ISO 7816 APDUs.

◆ dwPayLoadLen

uint32_t phalMfdfEVx_Sw_DataParams_t::dwPayLoadLen

Amount of data to be read.

Required for Enc read to verify CRC.

◆ bUid

uint8_t phalMfdfEVx_Sw_DataParams_t::bUid[15]

Complete UID of the PICC.

phalMfdfEVx_GetCardUID interface is called.

◆ bReturn_FabID

uint8_t phalMfdfEVx_Sw_DataParams_t::bReturn_FabID

Get / Set the return of Fabrication Identifier.

When Set will be utilized during GetVersion command exchange.


The documentation for this struct was generated from the following file: