NXP Reader Library  v17.1.0.2535
phalMfdfLight_SamAV3_NonX_DataParams_t Struct Reference

MIFARE DESfire Light SAM AV3 NonX parameter structure
More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_SamAV3_DataParams_tpHalSamDataParams
 Pointer to the parameter structure of the hal of the SAM layer.
 
void * pPalMifareDataParams
 Pointer to the parameter structure of the palMifare component.
 
phTMIUtils_tpTMIDataParams
 Pointer to the parameter structure for collecting TMI.
 
uint8_t bAuthMode
 Auth. More...
 
uint8_t bAuthType
 AuthType. More...
 
uint8_t bKeyNo
 Key number against which authenticated.
 
uint8_t pAid [3]
 Currently selected application Id.
 
uint16_t wAdditionalInfo
 Specific error codes for Desfire generic errors or error codes returned by the card.
 

Detailed Description

MIFARE DESfire Light SAM AV3 NonX parameter structure

Field Documentation

◆ bAuthMode

uint8_t phalMfdfLight_SamAV3_NonX_DataParams_t::bAuthMode

Auth.

Mode 0x0A or Ox1A or OxAA.

◆ bAuthType

uint8_t phalMfdfLight_SamAV3_NonX_DataParams_t::bAuthType

AuthType.

Whether its EV2 or LRP.


The documentation for this struct was generated from the following file: