NXP Reader Library  v17.1.0.2535
phalMfdf_SamAV2_X_DataParams_t Struct Reference

MIFARE DESfire SAM AV2 X parameter structure
More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_SamAV2_DataParams_tpHalSamDataParams
 Pointer to the parameter structure of the hal of the SAM layer.
 
uint8_t bAuthMode
 Auth Mode. More...
 
uint8_t bKeyNo
 Key number against which authenticated.
 
uint8_t bWrappedMode
 Wrapped APDU mode. More...
 
uint8_t pAid [3]
 Currently selected application Id.
 
uint16_t wAdditionalInfo
 Specific error codes for Desfire generic errors.
 

Detailed Description

MIFARE DESfire SAM AV2 X parameter structure

Field Documentation

◆ bAuthMode

uint8_t phalMfdf_SamAV2_X_DataParams_t::bAuthMode

Auth Mode.

0x0A or 0x1A or 0xAA.

◆ bWrappedMode

uint8_t phalMfdf_SamAV2_X_DataParams_t::bWrappedMode

Wrapped APDU mode.

All native commands need to be sent wrapped in ISO 7816 apdus.


The documentation for this struct was generated from the following file: