NXP Reader Library  v17.1.0.2535
phalMfpEVx_SamAV3_X_DataParams_t Struct Reference

MIFARE Plus EVx SamAV3 X parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_SamAV3_DataParams_tpHalSamDataParams
 Pointer to the parameter structure of the HAL layer of the SAM.
 
void * pPalMifareDataParams
 Pointer to the parameter structure of the palMifare component.
 
phTMIUtils_tpTMIDataParams
 Pointer to the parameter structure for collecting TMI.
 
uint8_t bAuthMode
 Security level authenticate.
 
uint8_t bSMMode
 Secure messaging mode. More...
 

Detailed Description

MIFARE Plus EVx SamAV3 X parameter structure.

Field Documentation

◆ bSMMode

uint8_t phalMfpEVx_SamAV3_X_DataParams_t::bSMMode

Secure messaging mode.

0: EV0 Mode; 1: EVx mode


The documentation for this struct was generated from the following file: