MIFARE Plus SamAV2 parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pPalMifareDataParams |
| Pointer to the parameter structure of the palMifare component. | |
| phhalHw_SamAV2_DataParams_t * | pHalSamDataParams |
| Pointer to the parameter structure of the hal of the SAM layer. | |
| uint8_t | bKeyModifier [PHAL_MFP_SIZE_KEYMODIFIER] |
| Key Modifier for MIFARE Plus SL2 authentication. | |
MIFARE Plus SamAV2 parameter structure.