NXP Reader Library  v17.1.0.2535
phalMful_SamAV3_NonX_DataParams_t Struct Reference

Data structure for MIFARE Ultralight / NTAG SAM AV3 NonX layer implementation
More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_SamAV3_DataParams_tpHalSamDataParams
 Pointer to halHw_SamAV3 parameter structure.
 
void * pPalMifareDataParams
 Pointer to palMifare parameter structure.
 
uint8_t bCMACReq
 Get/Set Config to include CMAC for required Commands.
 
uint16_t wCmdCtr
 Command count within transaction.
 
uint8_t bAuthMode
 Authentication PWD [0x1B] or AES [0x1A].
 
uint8_t bAdditionalInfo
 Specific error codes for MFUL generic errors or To get the response length of some commands.
 
uint8_t bRamKeyNo
 RAM KEY Number.
 
uint8_t bRamKeyVer
 RAM KEY Version.
 

Detailed Description

Data structure for MIFARE Ultralight / NTAG SAM AV3 NonX layer implementation


The documentation for this struct was generated from the following file: