NXP Reader Library  v17.1.0.2535
phalMful_SamAV3_X_DataParams_t Struct Reference

Data structure for MIFARE Ultralight / NTAG SAM AV3 X layer implementation
More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_SamAV3_DataParams_tpHalSamDataParams
 Pointer to halHw_SamAV3 parameter structure.
 
void * pPalMifareDataParams
 Pointer to palMifare_SamAV3_X parameter structure.
 
uint8_t bAdditionalInfo
 Specific error codes for MFUL generic errors or To get the response length of some commands.
 

Detailed Description

Data structure for MIFARE Ultralight / NTAG SAM AV3 X layer implementation


The documentation for this struct was generated from the following file: