NXP Reader Library  v17.1.0.2535
phalVca_SamAV2_DataParams_t Struct Reference

SAM AV2 NonX AL-VCA parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
void * pPalMifareDataParams
 Pointer to the parameter structure of the palMifare layer.
 
phhalHw_SamAV2_DataParams_tpSamHal
 Pointer to the parameter structure of the Sam HAL.
 
phalVca_SamAV2_CardTableEntry_tpCardTable
 Pointer to the Card Table of the layer.
 
uint16_t wCurrentCardTablePos
 Position of current entry in the CardTable.
 
uint16_t wNumCardTableEntries
 Number of Card table entries in the table.
 
uint8_tpRndq
 The memory storage is used to store RNDQ - Size: wNumCardTableEntries*12.
 
phalVca_SamAV2_KeyDuos_tpKeyDuos
 The memory storage is used to store Key duos.
 
uint8_t bNumKeyDuos
 Indicates the size of the key duos array.
 
uint8_t pPcdCaps [4]
 LenPcdCaps || PCD Caps.
 

Detailed Description

SAM AV2 NonX AL-VCA parameter structure.


The documentation for this struct was generated from the following file: