NXP Reader Library  v17.1.0.2535
phalVca_SamAV2_KeyDuos_t Struct Reference

Structure for KeyDuo Storage. More...

Data Fields

uint8_t bKeyEncNumber
 Number of encryption Key.
 
uint8_t bKeyEncVersion
 Version of encryption Key.
 
uint8_t bKeyMacNumber
 Number of MAC Key.
 
uint8_t bKeyMacVersion
 Version of MAC Key.
 

Detailed Description

Structure for KeyDuo Storage.


The documentation for this struct was generated from the following file: