NXP Reader Library  v17.1.0.2535
phalVca_SamAV3_NonX_DataParams_t Struct Reference

SAM AV3 NonX AL-VCA parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
void * pPalMifareDataParams
 Pointer to the parameter structure of the palMifare layer.
 
phhalHw_SamAV3_DataParams_tpSamHal
 Pointer to the parameter structure of the Sam Av3 HAL.
 
uint8_t bWrappedMode
 Wrapped APDU mode. More...
 
uint8_t bExtendedLenApdu
 Extended length APDU. More...
 
uint8_t bOption
 bOption parameter for Timing measurements ON/OFF.
 
uint16_t wAdditionalInfo
 Specific error codes for VC generic errors.
 

Detailed Description

SAM AV3 NonX AL-VCA parameter structure.

Field Documentation

◆ bWrappedMode

uint8_t phalVca_SamAV3_NonX_DataParams_t::bWrappedMode

Wrapped APDU mode.

All native commands need to be sent wrapped in ISO 7816 APDUs.

◆ bExtendedLenApdu

uint8_t phalVca_SamAV3_NonX_DataParams_t::bExtendedLenApdu

Extended length APDU.

If set the native commands should be wrapped in extended format


The documentation for this struct was generated from the following file: