NXP Reader Library  v17.1.0.2535
phalVca_Sw_CardTableEntry_t Struct Reference

Structure for Card table. More...

Data Fields

uint16_t wIidIndex
 Index of the associated IID.
 
uint8_t bValid
 Indicates if an entry is valid or not.
 
uint8_t pCardData [16]
 Card Data received from the Card.
 

Detailed Description

Structure for Card table.


The documentation for this struct was generated from the following file: