VCA Software parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pPalMifareDataParams |
| Pointer to the parameter structure of the palMifare component. | |
| void * | pKeyStoreDataParams |
| Pointer to the parameter structure of the KeyStore layer. | |
| void * | pCryptoDataParams |
| Pointer to the parameter structure of the Crypto layer. | |
| void * | pCryptoRngDataParams |
| Pointer to the parameter structure of the CryptoRng layer. | |
| phalVca_Sw_CardTableEntry_t * | pCardTable |
| Pointer to the Card Table of the layer. | |
| phalVca_Sw_IidTableEntry_t * | pIidTable |
| Pointer to the Iid Table of the layer. | |
| uint16_t | wCurrentCardTablePos |
| Position of current entry in the CardTable. | |
| uint16_t | wNumCardTableEntries |
| Number of Card table entries in the table. | |
| uint16_t | wNumIidTableEntries |
| Number of Iid table entries in the table. | |
| uint16_t | wCurrentIidIndex |
| Current index of the Iid sequence. | |
| uint16_t | wCurrentIidTablePos |
| Position of current entry in the Iid Table. | |
| uint16_t | wAdditionalInfo |
| Specific error codes for VC generic errors. | |
| uint8_t | bSessionAuthMACKey [16] |
| Session Keys for Authentication of MAC. | |
| phalVca_VirtualCardState | eVCState |
| Enum variable holding Virtual Card state. | |
| phalVca_ProximityCheckState | ePCState |
| Enum Variable holding Proximity Check state. | |
| void * | pAlDataParams |
| Pointer to the parameter structure of the DesfireEVx / MFPEVx component. | |
| uint8_t | bWrappedMode |
| Wrapped APDU mode. More... | |
| uint8_t | bExtendedLenApdu |
| Extended length APDU. More... | |
| uint8_t | bOption |
| bOption parameter for Timing measurements ON/OFF. | |
| uint8_t | bLowerBoundThreshold |
| parameter for enable/disable the LowerBound threshold time calculation(-20%). | |
VCA Software parameter structure.
| uint8_t phalVca_Sw_DataParams_t::bWrappedMode |
Wrapped APDU mode.
All native commands need to be sent wrapped in ISO 7816 APDUs.
| uint8_t phalVca_Sw_DataParams_t::bExtendedLenApdu |
Extended length APDU.
If set the native commands should be wrapped in extended format