NXP Reader Library  v17.1.0.2535
phalVca_Sw_IidTableEntry_t Struct Reference

Structure for IID table. More...

Data Fields

uint16_t wIidIndex
 Index of the associated IID.
 
uint16_t wKeyEncNumber
 Key number for Encryption key.
 
uint16_t wKeyEncVersion
 Key version for Encryption key.
 
uint16_t wKeyMacNumber
 Key number for MAC key.
 
uint16_t wKeyMacVersion
 Key version for MAC key.
 

Detailed Description

Structure for IID table.


The documentation for this struct was generated from the following file: