NXP Reader Library  v17.1.0.2535
phbalReg_PipeLin_DataParams_t Struct Reference

BAL PipeLin parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this BAL component, NEVER MODIFY!
 
uint8_t bMode
 Operating mode.
 
uint8_tpPipeNameRx
 Identifier of the named Rx-Pipe.
 
uint8_tpPipeNameTx
 Identifier of the named Tx-Pipe.
 
void * pPipeRx
 Pointer to RX communication pipe.
 
void * pPipeTx
 Pointer to TX communication pipe.
 
uint8_tpTxBuffer
 Pointer to global transmit buffer used by the Exchange() function.
 
uint16_t wTxBufSize
 Size of the global transmit buffer.
 
uint8_t bI2cSlaveAddr
 I2C slave address.
 
uint8_t bConfigValue
 current configuration value.
 

Detailed Description

BAL PipeLin parameter structure.


The documentation for this struct was generated from the following file: