NXP Reader Library  v17.1.0.2535
phhalHw_Rc663_DataParams_t Struct Reference

Rc663 HAL parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
void * pBalDataParams
 Pointer to the lower layers parameter structure.
 
uint8_t bLoadRegMode
 Whether LoadReg-Mode is enabled or not.
 
uint8_tpLoadRegConfig
 Pointer to configuration buffer for LoadReg mode; Refer to phhalHw_Rc663_Init.
 
uint8_tpTxBuffer
 Pointer to global transmit buffer used by the Exchange() function.
 
uint16_t wTxBufSize
 Size of the global transmit buffer.
 
uint16_t wTxBufLen
 Number of valid bytes within the transmit buffer.
 
uint8_tpRxBuffer
 Pointer to global receive buffer used by the Exchange() function.
 
uint16_t wRxBufSize
 Size of the global receive buffer.
 
uint16_t wRxBufLen
 Number of valid bytes within the receive buffer.
 
uint16_t wRxBufStartPos
 Starting position within the global receive buffer.
 
uint16_t wMaxPrecachedBytes
 Holds the max. More...
 
uint8_t bCardType
 Type of card for which the hal is configured for.
 
uint16_t wCfgShadow [PHHAL_HW_RC663_SHADOW_COUNT]
 Configuration shadow; Stores configuration for current cardtype.
 
uint16_t wTimingMode
 Current timing measurement mode.
 
uint8_t bTimeoutUnit
 Unit of current timeout value (either PHHAL_HW_TIME_MICROSECONDS or PHHAL_HW_TIME_MILLISECONDS).
 
uint32_t dwTimingUs
 Current timing value.
 
uint16_t wFieldOffTime
 Field-Off-Time in milliseconds.
 
uint16_t wFieldRecoveryTime
 Field-Recovery-Time in milliseconds.
 
uint8_t bSymbolStart
 Preamble of a frame.
 
uint8_t bSymbolEnd
 Trailer symbol of a frame.
 
uint8_t bFifoSize
 Fifo-Size setting.
 
uint16_t wAdditionalInfo
 Storage for additional error information.
 
uint8_t bBalConnectionType
 Type of the underlying BAL connection. More...
 
uint8_t bRfResetAfterTo
 Storage for PHHAL_HW_CONFIG_RFRESET_ON_TIMEOUT setting.
 
uint16_t dwFdtPc
 Current timing value backup for PC.
 

Detailed Description

Rc663 HAL parameter structure.

Field Documentation

◆ wMaxPrecachedBytes

uint16_t phhalHw_Rc663_DataParams_t::wMaxPrecachedBytes

Holds the max.

number of bytes which are precached prior to command execution.

◆ bBalConnectionType

uint8_t phhalHw_Rc663_DataParams_t::bBalConnectionType

Type of the underlying BAL connection.

Refer to PHHAL_HW_CONFIG_BAL_CONNECTION.


The documentation for this struct was generated from the following file: