NXP Reader Library  v17.1.0.2535
phhalHw_Rd70x_DataParams_t Struct Reference

Rd70x HAL parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phbalReg_Rd70xUsbWin_DataParams_tpBalDataParams
 pointer to the lower layers parameter structure
 
uint8_tpTxBuffer
 Pointer to global transmit buffer used by the Exchange() function.
 
uint16_t wTxBufSize
 Size of the global transmit buffer.
 
uint16_t wTxBufLen
 Number of valid bytes within the transmit buffer.
 
uint8_tpRxBuffer
 Pointer to global receive buffer used by the Exchange() function.
 
uint16_t wRxBufSize
 Size of the global receive buffer.
 
uint16_t wRxBufLen
 Number of valid bytes within the receive buffer.
 
uint16_t wRxBufStartPos
 Starting position within the global receive buffer.
 
uint16_t wTxBufStartPos
 Starting position within the global transmit buffer (used if TxBuffer equals RxBuffer).
 
uint8_t bCardType
 Type of card for which the hal is configured for.
 
uint16_t wCfgShadow [PHHAL_HW_RD70X_SHADOW_COUNT]
 Configuration shadow; Stores configuration for current cardtype.
 
uint16_t wTimingMode
 Current timing measurement mode.
 
uint32_t dwTimeoutUs
 TO value to be used with phhalHwRd700PiccExchgBitByte function.
 
uint32_t dwTimingUs
 Current timing value.
 
uint16_t wAdditionalInfo
 Storage for additional error information.
 
uint16_t wTxRxStartBackup
 Absolute Start-Position for transmission / reception used by buffer preservation mechanism.
 
uint16_t wFieldOffTime
 Field-Off-Time in milliseconds.
 
uint16_t wFieldRecoveryTime
 Field-Recovery-Time in milliseconds.
 
uint8_t bSymbolStart
 Preamble of a frame.
 
uint8_t bSymbolEnd
 Trailer symbol of a frame.
 
uint8_t bDisablePcdReset
 Whether to disable PcdReset call in phhalHw_ApplyProtocolSettings function or not.
 
uint8_t bFlags
 Flags to be used with phhalHwRd700PiccExchgBitByte function.
 
uint8_t bProtBuffer [PHHAL_HW_RD70X_RESERVED_BUFFER_LEN]
 Protocol buffer.
 
uint8_t bProtBufferLen
 Length of protocol data.
 
uint16_t wProtRxBufReadPos
 Read position within pRxBuffer for protocol.
 
uint8_t bRfResetAfterTo
 Storage for PHHAL_HW_CONFIG_RFRESET_ON_TIMEOUT setting.
 
uint8_t bTimerControlPc
 Backup for Timer control PC requirement.
 
uint16_t dwFdtPc
 Current timing value backup for PC.
 

Detailed Description

Rd70x HAL parameter structure.


The documentation for this struct was generated from the following file: