NXP Reader Library  v17.1.0.2535
phpalI14443p3a_Pcsc_DataParams_t Struct Reference

PAL-ISO14443P3A parameter structure for PCSC reader. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
void * pHalDataParams
 pointer to the parameter structure of the underlying layer
 
phbalReg_PcscWin_DataParams_tpBalDataParams
 pointer to the parameter structure of the underlying pcsc bal. More...
 
phhalHw_Pcsc_DataParams_tpHalPcscDataParams
 pointer to the parameter structure of the underlying pcsc hal. More...
 

Detailed Description

PAL-ISO14443P3A parameter structure for PCSC reader.

Field Documentation

◆ pBalDataParams

phbalReg_PcscWin_DataParams_t* phpalI14443p3a_Pcsc_DataParams_t::pBalDataParams

pointer to the parameter structure of the underlying pcsc bal.

Is used to access the pcsc parameter

◆ pHalPcscDataParams

phhalHw_Pcsc_DataParams_t* phpalI14443p3a_Pcsc_DataParams_t::pHalPcscDataParams

pointer to the parameter structure of the underlying pcsc hal.

Is used to access the pcsc parameter


The documentation for this struct was generated from the following file: