NXP Reader Library  v17.1.0.2535
phpalI14443p3a_SamAV2_X_DataParams_t Struct Reference

ISO14443-3A parameter structure for SAM AV2 X. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_SamAV2_DataParams_tpHalDataParams
 Pointer to the parameter structure of the underlying layer.
 
uint8_t abUid [10]
 Array holding the activated UID.
 
uint8_t bUidLength
 Length of UID stored in abUid.
 
uint8_t bUidComplete
 Whether the UID is complete (1) or not (0).
 

Detailed Description

ISO14443-3A parameter structure for SAM AV2 X.


The documentation for this struct was generated from the following file: