NXP Reader Library  v17.1.0.2535
phpalI14443p4_Pcsc_DataParams_t Struct Reference

PCSC ISO14443-4 parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
void * pHalDataParams
 Pointer to the parameter structure of the underlying layer.
 
phbalReg_PcscWin_DataParams_tpBalDataParams
 pointer to the parameter structure of the underlying pcsc bal. More...
 
phhalHw_Pcsc_DataParams_tpHalPcscDataParams
 pointer to the parameter structure of the underlying pcsc hal. More...
 
uint8_t bStateNow
 Current Exchange-State.
 
uint8_t bCidEnabled
 Card Identifier Enabler; Unequal '0' if enabled.
 
uint8_t bCid
 Card Identifier; Ignored if *pCidSupported is equal '0'.
 
uint8_t bNadEnabled
 Node Address Enabler; Unequal '0' if enabled.
 
uint8_t bNad
 Node Address; Ignored if bNadEnabled is equal '0'.
 
uint8_t bFwi
 Frame Waiting Integer.
 
uint8_t bFsdi
 PCD Frame Size Integer; 0-8;.
 
uint8_t bFsci
 PICC Frame Size Integer; 0-8;.
 
uint8_t bPcbBlockNum
 Current Block-Number; 0/1;.
 
uint8_t bMaxRetryCount
 Maximum Retry count for ISO/IEC 14443-4:2008(E) Rule 4 and 5.
 
uint8_t bExchangeType
 Type of exchange to use. More...
 

Detailed Description

PCSC ISO14443-4 parameter structure.

Field Documentation

◆ pBalDataParams

phbalReg_PcscWin_DataParams_t* phpalI14443p4_Pcsc_DataParams_t::pBalDataParams

pointer to the parameter structure of the underlying pcsc bal.

Is used to access the pcsc parameter

◆ pHalPcscDataParams

phhalHw_Pcsc_DataParams_t* phpalI14443p4_Pcsc_DataParams_t::pHalPcscDataParams

pointer to the parameter structure of the underlying pcsc hal.

Is used to access the pcsc parameter

◆ bExchangeType

uint8_t phpalI14443p4_Pcsc_DataParams_t::bExchangeType

Type of exchange to use.

PHPAL_I14443P4_PCSC_NORMAL (default) or PHPAL_I14443P4_PCSC_TRANSPARENT.


The documentation for this struct was generated from the following file: