NXP Reader Library
v17.1.0.2535
Data Fields
phpalI14443p4_SamAV3_X_DataParams_t Struct Reference
Protocol Abstraction Layer
»
ISO/IEC14443-4
»
Component : SamAV3_X
ISO14443-4 parameter structure.
More...
Data Fields
uint16_t
wId
Layer ID for this component, NEVER MODIFY!
phhalHw_SamAV3_DataParams_t
*
pHalDataParams
pointer to the parameter structure of the underlying layer.
Detailed Description
ISO14443-4 parameter structure.
The documentation for this struct was generated from the following file:
phpalI14443p4.h
phpalI14443p4_SamAV3_X_DataParams_t
Generated on Sun Aug 31 2025 16:24:00 for NXP Reader Library by © NXP 2021