NXP Reader Library  v17.1.0.2535
phpalI14443p4a_SamAV2_X_DataParams_t Struct Reference

ISO14443-4a parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!

 
phhalHw_SamAV2_DataParams_tpHalDataParams
 pointer to the parameter structure of the underlying layer
 
uint8_t bCidSupported
 Cid Support indicator; Unequal '0' if supported. More...
 
uint8_t bNadSupported
 Nad Support indicator; Unequal '0' if supported. More...
 
uint8_t bCid
 Card Identifier; Ignored if bCidSupported is equal '0'. More...
 
uint8_t bBitRateCaps
 TA(1) byte of ATS; ISO/IEC 14443-4:2008, Section 5.2.4

 
uint8_t bFwi
 Frame Waiting Integer. More...
 
uint8_t bFsci
 PICC Frame Size Integer; 0-8

 
uint8_t bDri
 (Current) Divisor Receive (PCD to PICC) Integer; 0-3

 
uint8_t bDsi
 (Current) Divisor Send (PICC to PCD) Integer; 0-3

 

Detailed Description

ISO14443-4a parameter structure.

Field Documentation

◆ bCidSupported

uint8_t phpalI14443p4a_SamAV2_X_DataParams_t::bCidSupported

Cid Support indicator; Unequal '0' if supported.


◆ bNadSupported

uint8_t phpalI14443p4a_SamAV2_X_DataParams_t::bNadSupported

Nad Support indicator; Unequal '0' if supported.


◆ bCid

uint8_t phpalI14443p4a_SamAV2_X_DataParams_t::bCid

Card Identifier; Ignored if bCidSupported is equal '0'.


◆ bFwi

uint8_t phpalI14443p4a_SamAV2_X_DataParams_t::bFwi

Frame Waiting Integer.



The documentation for this struct was generated from the following file: