NXP Reader Library  v17.1.0.2535
phpalI18000p3m3_Sw_DataParams_t Struct Reference

Software PAL-I18000P3M3 parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
void * pHalDataParams
 Pointer to the parameter structure of the underlying HAL layer.
 
uint8_t bSession
 Active session of invertory round.
 
uint8_t abStoredCRC [2]
 Stored CRC returned by the tag.
 
uint8_t bStoredCRCValid
 Whether StoredCRC is valid or not.
 

Detailed Description

Software PAL-I18000P3M3 parameter structure.


The documentation for this struct was generated from the following file: