NXP Reader Library  v17.1.0.2535
KeyStore

This is only a wrapper layer to abstract the different KeyStore implementations. With this wrapper it is possible to support more than one CryptoSym implementation in parallel, by adapting this wrapper. More...

Collaboration diagram for KeyStore:

Modules

 Component : Software
 KeyStore implementation in Software.
 
 Component : Rc663
 KeyStore implementation to use RC663 Hardware KeyStore.
 
 Component : Rc632
 KeyStore implementation to use RC632 Hardware KeyStore.
 
 Component : Rd710
 KeyStore implementation to use RD710 Hardware KeyStore.
 
 Defines
 Definitions for KeyStore layer.
 
 Symmetric
 Interfaces for Symmetric keys of KeyStore component.
 
 ASymmetric
 Interfaces for ASymmetric keys of KeyStore component.
 
 Utility
 Interfaces for utility interfaces for KeyStore component.
 

Functions

phStatus_t phKeyStore_FormatKeyEntry (void *pDataParams, uint16_t wKeyNo, uint16_t wNewKeyType)
 Format a key entry to a new KeyType. More...
 
phStatus_t phKeyStore_SetKUC (void *pDataParams, uint16_t wKeyNo, uint16_t wRefNoKUC)
 Change the KUC of a key entry. More...
 
phStatus_t phKeyStore_GetKUC (void *pDataParams, uint16_t wRefNoKUC, uint32_t *pdwLimit, uint32_t *pdwCurVal)
 Obtain a key usage counter entry. More...
 
phStatus_t phKeyStore_ChangeKUC (void *pDataParams, uint16_t wRefNoKUC, uint32_t dwLimit)
 Change a key usage counter entry. More...
 
phStatus_t phKeyStore_SetConfig (void *pDataParams, uint16_t wConfig, uint16_t wValue)
 Set configuration parameter. More...
 
phStatus_t phKeyStore_SetConfigStr (void *pDataParams, uint16_t wConfig, uint8_t *pBuffer, uint16_t wBufferLength)
 Set configuration parameter. More...
 
phStatus_t phKeyStore_GetConfig (void *pDataParams, uint16_t wConfig, uint16_t *pValue)
 Get configuration parameter. More...
 
phStatus_t phKeyStore_GetConfigStr (void *pDataParams, uint16_t wConfig, uint8_t **ppBuffer, uint16_t *pBufferLength)
 Get configuration parameter. More...
 

Detailed Description

This is only a wrapper layer to abstract the different KeyStore implementations. With this wrapper it is possible to support more than one CryptoSym implementation in parallel, by adapting this wrapper.

Important hints for users of this component:

Function Documentation

◆ phKeyStore_FormatKeyEntry()

phStatus_t phKeyStore_FormatKeyEntry ( void *  pDataParams,
uint16_t  wKeyNo,
uint16_t  wNewKeyType 
)

Format a key entry to a new KeyType.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wKeyNo[In] KeyEntry number to be Formatted.
[in]wNewKeyType[In] New Key type of the KeyEntry (predefined type of KeyType).

◆ phKeyStore_SetKUC()

phStatus_t phKeyStore_SetKUC ( void *  pDataParams,
uint16_t  wKeyNo,
uint16_t  wRefNoKUC 
)

Change the KUC of a key entry.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wKeyNo[In] KeyEntry number.
[in]wRefNoKUC[In] Reference Number of the key usage counter used together with that key.

◆ phKeyStore_GetKUC()

phStatus_t phKeyStore_GetKUC ( void *  pDataParams,
uint16_t  wRefNoKUC,
uint32_t pdwLimit,
uint32_t pdwCurVal 
)

Obtain a key usage counter entry.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wRefNoKUC[In] Number of the key usage counter to be looked at (00h to 0Fh)
[out]pdwLimit[Out] Currently Set Limit in the KUC
[out]pdwCurVal[Out] Currently set value in the KUC

◆ phKeyStore_ChangeKUC()

phStatus_t phKeyStore_ChangeKUC ( void *  pDataParams,
uint16_t  wRefNoKUC,
uint32_t  dwLimit 
)

Change a key usage counter entry.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wRefNoKUC[In] Number of key entry.
[in]dwLimit[In] Limit of the Key Usage Counter.

◆ phKeyStore_SetConfig()

phStatus_t phKeyStore_SetConfig ( void *  pDataParams,
uint16_t  wConfig,
uint16_t  wValue 
)

Set configuration parameter.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wConfig[In] Configuration Identifier
[in]wValue[In] Configuration Value

◆ phKeyStore_SetConfigStr()

phStatus_t phKeyStore_SetConfigStr ( void *  pDataParams,
uint16_t  wConfig,
uint8_t pBuffer,
uint16_t  wBufferLength 
)

Set configuration parameter.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wConfig[In] Configuration Identifier.
[in]pBuffer[In] Buffer containing the configuration string.
[in]wBufferLength[In] Length of configuration string.

◆ phKeyStore_GetConfig()

phStatus_t phKeyStore_GetConfig ( void *  pDataParams,
uint16_t  wConfig,
uint16_t pValue 
)

Get configuration parameter.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wConfig[In] Configuration Identifier
[out]pValue[Out] Configuration Value

◆ phKeyStore_GetConfigStr()

phStatus_t phKeyStore_GetConfigStr ( void *  pDataParams,
uint16_t  wConfig,
uint8_t **  ppBuffer,
uint16_t pBufferLength 
)

Get configuration parameter.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wConfig[In] Configuration Identifier
[out]ppBuffer[Out] Pointer to the buffer containing the configuration string.
[out]pBufferLength[Out] Amount of valid bytes in the configuration string buffer.