Generic component that provides the command description of ICode products. More...

Modules | |
| Component : Software | |
| Sub-Component to initialize ICode Generic component as Software. | |
| ErrorCodes | |
| Description of error codes returned by VICC and Reader Library. | |
| Defines | |
| Describes about the macro definitions supported / to be used in the interfaces. | |
| Commands_Mandatory | |
| Describes the Mandatory commands of ICode products. | |
| Commands_Optional | |
| Describes the Optional commands of ICode products. | |
| Commands_Custom | |
| Describes the Custom commands of ICode products. | |
| Utilities | |
| Describes the utility interfaces. These interfaces are actually not of ISO15693 or any of the ICode product families. These are generic interfaces as part of reader library for internal purpose. | |
Generic component that provides the command description of ICode products.