NXP Reader Library  v17.1.0.2535

This is only a wrapper layer to abstract the different MIFARE DUOX implementations. With this wrapper it is possible to support more than one MIFARE DUOX implementation in parallel, by adapting this wrapper. More...

Collaboration diagram for MIFARE DUOX:

Modules

 Component : Software
 Software implementation of the MIFARE DUOX commands. Here the MIFARE DUOX commands are framed and exchanged to PICC.
 
 ErrorCodes
 Error Codes received from PICC and the equivalent Reader Library error codes.
 
 Defines
 
 Commands_SecureMessaging
 Describes about the MIFARE DUOX Secure Messaging related commands.
 
 Commands_MemoryConfiguration
 Describes about the MIFARE DUOX Memory and Configuration Management commands.
 
 Commands_SymmetricKeyManagement
 Describes about the MIFARE DUOX Symmetric Key Management commands.
 
 Commands_ASymmetricKeyManagement
 Describes about the MIFARE DUOX ASymmetric Key Management commands.
 
 Commands_ApplicationManagement
 Describes about the MIFARE DUOX Application Management commands.
 
 Commands_FileManagement
 Describes about the MIFARE DUOX File Management commands.
 
 Commands_DataManagement
 Describes about the MIFARE DUOX Data Management commands.
 
 Commands_TransactionManagement
 Describes about the MIFARE DUOX Transaction Management commands.
 
 Commands_CryptographicSupport
 Describes about the MIFARE DUOX Cryptographic Support commands.
 
 Commands_GPIOManagement
 Describes about the MIFARE DUOX GPIO commands.
 
 Commands_ISO7816
 Describes about the MIFARE DUOX ISO/IEC 7816-4 Standard commands.
 
 Commands_EVCharging
 Describes about the MIFARE DUOX EV Charging commands.
 
 Commands_Utility
 Describes about the MIFARE DUOX Utility functions. These are not part of actual MIFARE DUOX data sheet rather its for internal purpose.
 

Detailed Description

This is only a wrapper layer to abstract the different MIFARE DUOX implementations. With this wrapper it is possible to support more than one MIFARE DUOX implementation in parallel, by adapting this wrapper.

Note