NXP Reader Library  v17.1.0.2535

Macro Definitions for File Management commands. More...

Collaboration diagram for Defines:

Modules

 FileOptions
 The File Options to be used for all the File management commands.
 
 LimitedCredit
 The File Options to be used for Create Value File interface.
 
 GetValue
 The File Options to be used for Create Value File interface.
 
 CommandCodes
 

Detailed Description

Macro Definitions for File Management commands.