NXP Reader Library  v17.1.0.2535
MIFARE DESFire Light

These Functions implement the MIFARE DESFire Light commands. More...

Collaboration diagram for MIFARE DESFire Light:

Modules

 Component : Software
 
 Error Codes
 Lists the PICC response codes and equivalent library codes that correponds to PICC Return code.
 
 Commands_SecureMessaging
 These Components implement the MIFARE DESFire Light Secure Messaging related commands.
 
 Commands_MemoryConfiguration
 These Components implement the MIFARE DESFire Light Memory and Configuration Management related commands.
 
 Commands_KeyManagement
 These Components implement the MIFARE DESFire Light Key Management related commands.
 
 Commands_FileManagement
 These Components implement the MIFARE DESFire Light File Management related commands.
 
 Commands_DataManagement
 These Components implement the MIFARE DESFire Light Data Management related commands.
 
 Commands_TransactionManagement
 These Components implement the MIFARE DESFire Light Transaction Management related commands.
 
 Commands_ISO7816
 These Components implement the MIFARE DESFire Light ISO/IEC 7816-4 Basic commands.
 
 Commands_OriginalityCheck
 These Components implement the MIFARE DESFire Light Originality Check functions.
 
 Commands_Miscellaneous
 These Components implement the MIFARE DESFire Light Miscellaneous functions. These are not part of actual DESFire Light data sheet rather its for internal purpose.
 

Other Options for various Functions

#define PHAL_MFDFLIGHT_ORIGINALITY_KEY_FIRST   0x01U
 Originality key for AES.
 
#define PHAL_MFDFLIGHT_ORIGINALITY_KEY_LAST   0x04U
 Originality key for AES

 
#define PHAL_MFDFLIGHT_APP_KEY_LAST   0x04U
 Numebr of application keys.
 
#define PHAL_MFDFLIGHT_MAC_DATA_INCOMPLETE   0x01U
 Option for indicating more data to come in next call for MAC calculation.
 
#define PHAL_MFDFLIGHT_COMMUNICATION_MAC_ON_RC   0x02U
 MAC is appended over response

 
#define PHAL_MFDFLIGHT_AUTHENTICATE_RESET   0x08U
 authentication state shall be reset
 

The communication mode to be used.

#define PHAL_MFDFLIGHT_COMMUNICATION_PLAIN   0x00U
 Plain mode of communication.
 
#define PHAL_MFDFLIGHT_COMMUNICATION_PLAIN_1   0x20U
 Plain mode of communication.
 
#define PHAL_MFDFLIGHT_COMMUNICATION_MACD   0x10U
 MAC mode of communication.
 
#define PHAL_MFDFLIGHT_COMMUNICATION_ENC   0x30U
 Enciphered mode of communication.
 

Key Types

#define PHAL_MFDFLIGHT_KEY_TYPE_2K3DES   0x00U
 2 Key Triple Des
 
#define PHAL_MFDFLIGHT_KEY_TYPE_3K3DES   0x01U
 3 Key Triple Des
 
#define PHAL_MFDFLIGHT_KEY_TYPE_AES128   0x02U
 AES 128 Key.
 

MIFARE DESFire Light Native Commands

#define PHAL_MFDFLIGHT_CMD_AUTHENTICATE_EV2_FIRST   0x71
 MFDFLIGHT Authenticate Ev2 First command.
 
#define PHAL_MFDFLIGHT_CMD_AUTHENTICATE_EV2_NON_FIRST   0x77
 MFDFLIGHT Authenticate Ev2 Non First command.
 
#define PHAL_MFDFLIGHT_CMD_CHANGE_KEY   0xC4
 MFDFLIGHT Change key cmd.
 
#define PHAL_MFDFLIGHT_CMD_GET_KEY_VERSION   0x64
 MFDFLIGHT Get Key Version.
 
#define PHAL_MFDFLIGHT_CMD_GET_VERSION   0x60
 MFDFLIGHT Get Version cmd.
 
#define PHAL_MFDFLIGHT_CMD_SET_CONFIG   0x5C
 MFDFLIGHT Set Configuration Cmd.
 
#define PHAL_MFDFLIGHT_CMD_GET_CARD_UID   0x51
 MFDFLIGHT Get Card UID cmd.
 
#define PHAL_MFDFLIGHT_CMD_DELETE_APPLN   0xDA
 MFDFLIGHT Delete Application cmd.
 
#define PHAL_MFDFLIGHT_CMD_GET_FILE_IDS   0x6F
 MFDFLIGHT Get File IDs cmd.
 
#define PHAL_MFDFLIGHT_CMD_GET_ISO_FILE_IDS   0x61
 MFDFLIGHT Get ISO File IDs cmd.
 
#define PHAL_MFDFLIGHT_CMD_GET_FILE_SETTINGS   0xF5
 MFDFLIGHT Get File settings cmd.
 
#define PHAL_MFDFLIGHT_CMD_CHANGE_FILE_SETTINGS   0x5F
 MFDFLIGHT Change file settings cmd.
 
#define PHAL_MFDFLIGHT_CMD_CREATE_TRANSACTION_MACFILE   0xCE
 MFDFLIGHT Create Transaction MAC file cmd.
 
#define PHAL_MFDFLIGHT_CMD_DELETE_FILE   0xDF
 MFDFLIGHT Delete File cmd.
 
#define PHAL_MFDFLIGHT_CMD_READ_DATA   0xBD
 MFDFLIGHT Read Data cmd.
 
#define PHAL_MFDFLIGHT_CMD_READ_DATA_ISO   0xAD
 MFDFLIGHT Read Data cmd using ISO chaining.
 
#define PHAL_MFDFLIGHT_CMD_WRITE_DATA   0x3D
 MFDFLIGHT Write data cmd.
 
#define PHAL_MFDFLIGHT_CMD_WRITE_DATA_ISO   0x8D
 MFDFLIGHT Write data cmd using ISO chaining.
 
#define PHAL_MFDFLIGHT_CMD_GET_VALUE   0x6C
 MFDFLIGHT Get Value cmd.
 
#define PHAL_MFDFLIGHT_CMD_CREDIT   0x0C
 MFDFLIGHT Credit cmd.
 
#define PHAL_MFDFLIGHT_CMD_DEBIT   0xDC
 MFDFLIGHT Debit cmd.
 
#define PHAL_MFDFLIGHT_CMD_LIMITED_CREDIT   0x1C
 MFDFLIGHT Limited Credit cmd.
 
#define PHAL_MFDFLIGHT_CMD_WRITE_RECORD   0x3B
 MFDFLIGHT Write Record cmd.
 
#define PHAL_MFDFLIGHT_CMD_WRITE_RECORD_ISO   0x8B
 MFDFLIGHT Write Record cmd using ISO chaining.
 
#define PHAL_MFDFLIGHT_CMD_UPDATE_RECORD   0xDB
 MFDFLIGHT Update Record cmd.
 
#define PHAL_MFDFLIGHT_CMD_UPDATE_RECORD_ISO   0xBA
 MFDFLIGHT Update Record cmd using ISO chaining.
 
#define PHAL_MFDFLIGHT_CMD_READ_RECORDS   0xBB
 MFDFLIGHT Read Records cmd.
 
#define PHAL_MFDFLIGHT_CMD_READ_RECORDS_ISO   0xAB
 MFDFLIGHT Read Records cmd using ISO chaining.
 
#define PHAL_MFDFLIGHT_CMD_CLEAR_RECORD_FILE   0xEB
 MFDFLIGHT Clear records file cmd.
 
#define PHAL_MFDFLIGHT_CMD_COMMIT_TXN   0xC7
 MFDFLIGHT Commit transaction cmd.
 
#define PHAL_MFDFLIGHT_CMD_ABORT_TXN   0xA7
 MFDFLIGHT Abort transaction cmd.
 
#define PHAL_MFDFLIGHT_CMD_COMMIT_READER_ID   0xC8
 MFDFLIGHT Commit Reader ID cmd.
 
#define PHAL_MFDFLIGHT_CMD_READ_SIG   0x3C
 MFDFLIGHT Verify read signature command.
 
#define PHAL_MFDFLIGHT_CMD_CLEAR_RECORDS_FILE   0xEB
 MFDFLIGHT Clear records file cmd.
 

MIFARE DESFire Light ISO7816 Commands

#define PHAL_MFDFLIGHT_CMD_ISO7816_SELECT_FILE   0xA4
 ISO Select File.
 
#define PHAL_MFDFLIGHT_CMD_ISO7816_READ_BINARY   0xB0
 ISO Read Binary.
 
#define PHAL_MFDFLIGHT_CMD_ISO7816_UPDATE_BINARY   0xD6
 ISO UPDATE Binary.
 
#define PHAL_MFDFLIGHT_CMD_ISO7816_APPEND_RECORD   0xE2
 ISO Append record.
 
#define PHAL_MFDFLIGHT_CMD_ISO7816_UPDATE_RECORD   0xD2
 ISO Update record.
 

Detailed Description

These Functions implement the MIFARE DESFire Light commands.