NXP Reader Library  v17.1.0.2535
MIFARE Plus EVx

These Components implement the MIFARE Plus (EVx, EV2, future versions) commands. More...

Collaboration diagram for MIFARE Plus EVx:

Modules

 Component : Software
 
 ErrorCodes
 These component implement the MIFARE Plus (EVx, EV2, future versions) Error codes.
 
 Common Definitions
 These are common definitions for most of the Plus commands.
 
 Commands_Personalization
 These Components implement the MIFARE Plus EVx personalization commands.
 
 Commands_Authenticate
 These Components implement the MIFARE Plus EVx authentication commands.
 
 Commands_Special
 These Components implement the MIFARE Plus EVx additional feature commands.
 
 Utilities
 These Components implement the utility interfaces required for MIFARE Plus EVx application layer. These are not commands.
 

Detailed Description

These Components implement the MIFARE Plus (EVx, EV2, future versions) commands.