NXP Reader Library  v17.1.0.2535

These Components implement the MIFARE Plus EVx additional feature commands. More...

Collaboration diagram for Commands_Special:

Functions

phStatus_t phalMfpEVx_GetVersion (void *pDataParams, uint8_t *pVerInfo)
 Returns manufacturing related data of the PICC. More...
 
phStatus_t phalMfpEVx_ReadSign (void *pDataParams, uint8_t bLayer4Comm, uint8_t bAddr, uint8_t **pSignature)
 Read originality Signature from the PICC. More...
 
phStatus_t phalMfpEVx_ResetAuth (void *pDataParams)
 Performs a Reset Authentication command. More...
 
phStatus_t phalMfpEVx_PersonalizeUid (void *pDataParams, uint8_t bUidType)
 Perform MIFARE(R) Personalize UID usage command sequence with MIFARE Picc. More...
 
phStatus_t phalMfpEVx_SetConfigSL1 (void *pDataParams, uint8_t bOption)
 Performs a configuration for ISO1443-4 enabling in Security Level 1. More...
 
phStatus_t phalMfpEVx_ReadSL1TMBlock (void *pDataParams, uint16_t wBlockNr, uint8_t *pBlocks)
 Performs read of the TMAC block in security layer 1 with ISO14443 Layer 3 activated. More...
 
phStatus_t phalMfpEVx_VCSupportLastISOL3 (void *pDataParams, uint8_t *pIid, uint8_t *pPcdCapL3, uint8_t *pInfo)
 Performs a VCSupportLastISOL3 command operation. More...
 

Options to personalize the UID.

#define PHAL_MFPEVX_UID_TYPE_UIDF0   0x00U
 MIFARE(R) Plus EVx UID type UIDF0.
 
#define PHAL_MFPEVX_UID_TYPE_UIDF1   0x40U
 MIFARE(R) Plus EVx UID type UIDF1.
 
#define PHAL_MFPEVX_UID_TYPE_UIDF2   0x20U
 MIFARE(R) Plus EVx UID type UIDF2.
 
#define PHAL_MFPEVX_UID_TYPE_UIDF3   0x60U
 MIFARE(R) Plus EVx UID type UIDF3.
 

Options to Enable / Disable ISO14443 Layer 4 protocol.

#define PHAL_MFPEVX_ENABLE_ISO14443_L4   0x00U
 Option to enable ISO14443 Layer 4 protocol.
 
#define PHAL_MFPEVX_DISABLE_ISO14443_L4   0x01U
 Option to disable ISO14443 Layer 4 protocol.
 

Detailed Description

These Components implement the MIFARE Plus EVx additional feature commands.

Function Documentation

◆ phalMfpEVx_GetVersion()

phStatus_t phalMfpEVx_GetVersion ( void *  pDataParams,
uint8_t pVerInfo 
)

Returns manufacturing related data of the PICC.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[out]pVerInfo[Out] The version information of the PICC.
If UID is 4 bytes, the buffer will have 27 bytes of version information.
If UID is 7 bytes, the buffer will have 28 bytes of version information.
If UID is 10 bytes, the buffer will have 33 bytes of version information.

◆ phalMfpEVx_ReadSign()

phStatus_t phalMfpEVx_ReadSign ( void *  pDataParams,
uint8_t  bLayer4Comm,
uint8_t  bAddr,
uint8_t **  pSignature 
)

Read originality Signature from the PICC.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bLayer4Comm[In] ISO14443 protocol to be used.
[in]bAddr[In] Targeted ECC originality check signature.
[out]pSignature[Out] PICC's orginality signature. The buffer will have 56 bytes of signature information.

◆ phalMfpEVx_ResetAuth()

phStatus_t phalMfpEVx_ResetAuth ( void *  pDataParams)

Performs a Reset Authentication command.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.

◆ phalMfpEVx_PersonalizeUid()

phStatus_t phalMfpEVx_PersonalizeUid ( void *  pDataParams,
uint8_t  bUidType 
)

Perform MIFARE(R) Personalize UID usage command sequence with MIFARE Picc.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bUidType[In] UID type to be used for personalization.

◆ phalMfpEVx_SetConfigSL1()

phStatus_t phalMfpEVx_SetConfigSL1 ( void *  pDataParams,
uint8_t  bOption 
)

Performs a configuration for ISO1443-4 enabling in Security Level 1.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bOption[In] Option byte encoding the configuration to be set.

◆ phalMfpEVx_ReadSL1TMBlock()

phStatus_t phalMfpEVx_ReadSL1TMBlock ( void *  pDataParams,
uint16_t  wBlockNr,
uint8_t pBlocks 
)

Performs read of the TMAC block in security layer 1 with ISO14443 Layer 3 activated.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wBlockNr[In] PICC TM block number from which the data should be read.
[out]pBlocks[Out] The data read from the specified block number. The buffer will contain 16 bytes information.

◆ phalMfpEVx_VCSupportLastISOL3()

phStatus_t phalMfpEVx_VCSupportLastISOL3 ( void *  pDataParams,
uint8_t pIid,
uint8_t pPcdCapL3,
uint8_t pInfo 
)

Performs a VCSupportLastISOL3 command operation.

This command is a special variant of virtual card operation. This command can be sent after a ISO14443-3 activation.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]pIid[In] The (last) IID that the PCD presents to the PD. The buffer should have 16 bytes of information.
[in]pPcdCapL3[In] Capability vector of the PCD. The buffer should have 4 bytes of information.
[out]pInfo[Out] One byte Information returned by PICC.