NXP Reader Library
v17.1.0.2535
Data Fields
phalVca_Sw_CardTableEntry_t Struct Reference
Application Layer
»
Virtual Card Architecture (R)
»
Component : Software
Structure for Card table.
More...
Data Fields
uint16_t
wIidIndex
Index of the associated IID.
uint8_t
bValid
Indicates if an entry is valid or not.
uint8_t
pCardData
[16]
Card Data received from the Card.
Detailed Description
Structure for Card table.
The documentation for this struct was generated from the following file:
phalVca.h
phalVca_Sw_CardTableEntry_t
Generated on Sun Aug 31 2025 16:26:29 for NXP Reader Library by © NXP 2021