==============================================================================
Readme - Source Package for CL RD710
==============================================================================

1. Document purpose

This document describes the content of the source package of
the CL RD710 as well as known problems and restrictions.
A separate User Manual describes the first steps how to use the software in
combination with the Hardware.


2. Known problems and restrictions

* Restrictions
The Software is restricted to the Hardware, described in the attached
schematics. The API is intended for the NXP contactless/contact reader ICs, 
as such the API is not to be ported to any technology from any other vendor.
The Software is running on a MFRC523 controller from NXP. 
NXP will not support porting to any other vendor platform. 

* Known Problems

  - None
	
3. Content


EULA.pdf (EULA - End User License Agreement)

CLRD710_driver_patch.zip (Files for implemtation of own Pegoda Driver)

CLRD710 FW_v1_3.zip (Firmware source code and project file for FW Version 1.3)

CLRD710 FW_v2_2.zip (Firmware source code and project file for FW Version 2.2)

CLRD710 PCB Design.zip (Schematics)

FW_Release_Notes_v2_2.pdf (Release Notes and Update recommendation for Firmware Version 2.2)

Readme.txt (this document)

4. Documentation material, not included

	
All additionally available documentation can be downloaded at: 
http://www.nxp.com/demoboard/MFEV710.html#documentation


5. Revision History

V1.0.0.0 (Build 10082012):
* First packaged version.