Freescale Semiconductor
V.22bis Calling Modem Example Application for 5685x
Overview
In this demo, the V.22bis application is connected to a standard modem to test for interoperability.
In this application, V.22bis calls another modem and creates a data-pump to demonstrate
text / data transfer between two hosts using HyperTerminal.
How to get this software
This example application is included as part of the CodeWarrior Development Studio for 56800/E Digital
Signal Controllers. Follow these steps:
1. Install CodeWarrior Development Studio for 56800/E Digital Signal Controllers
2. Launch CodeWarrior, and create new Processor Expert project
a. Select File > New menu
b. Select Processor Expert Examples Stationery
c. Type project name
d. Click OK
e. Select DemoApplications > Modem > v22bis > 56858 > InterOpCall
f. Click OK
3. Generate application code by selecting Processor Expert > Generate Code menu
Detailed documentation
Documentation for this application is included as part of this example project. Expand Doc folder located
in the project window by clicking on the + icon next to the folder, and open desired file by double clicking it.
Freescale™ and the Freescale logo are trademarks of Freescale Semiconductor, Inc. All other product
or service names are the property of their respective owners. 
©2005, Freescale Semiconductor, Inc