| Freescale Semiconductor | |||||||||||||
| V.22bis Calling Modem Example Application for 5685x | |||||||||||||
| Overview | |||||||||||||
| In this demo, the V.22bis application is connected to a standard modem to test for interoperability. | |||||||||||||
| In this application, V.22bis calls another modem and creates a data-pump to demonstrate | |||||||||||||
| text / data transfer between two hosts using HyperTerminal. | |||||||||||||
| How to get this software | |||||||||||||
| This example application is included as part of the CodeWarrior Development Studio for 56800/E Digital | |||||||||||||
| Signal Controllers. Follow these steps: | |||||||||||||
| 1. | Install CodeWarrior Development Studio for 56800/E Digital Signal Controllers | ||||||||||||
| 2. | Launch CodeWarrior, and create new Processor Expert project | ||||||||||||
| a. | Select File > New menu | ||||||||||||
| b. | Select Processor Expert Examples Stationery | ||||||||||||
| c. | Type project name | ||||||||||||
| d. | Click OK | ||||||||||||
| e. | Select DemoApplications > Modem > v22bis > 56858 > InterOpCall | ||||||||||||
| f. | Click OK | ||||||||||||
| 3. | Generate application code by selecting Processor Expert > Generate Code menu | ||||||||||||
| Detailed documentation | |||||||||||||
| Documentation for this application is included as part of this example project. Expand Doc folder located | |||||||||||||
| in the project window by clicking on the + icon next to the folder, and open desired file by double clicking it. | |||||||||||||
| Freescale™ and the Freescale logo are trademarks of Freescale Semiconductor, Inc. All other product | |||||||||||||
| or service names are the property of their respective owners. | |||||||||||||
| ©2005, Freescale Semiconductor, Inc | |||||||||||||