| Freescale Semiconductor | ||||||||||||
| Common Tone Generation (CTG) Example Application for 56F82x | ||||||||||||
| Overview | ||||||||||||
| The Common Tone Generation Demo, which runs on the 56F82x platform, generates North American | ||||||||||||
| Call Progress Tones with specifications for: | ||||||||||||
| | Dial Tone | |||||||||||
| | Message Waiting Indicator Tone | |||||||||||
| | Recall Dial Tone / Confirmation Tone. | |||||||||||
| | Line Busy Tone | |||||||||||
| | Re-Order Tone | |||||||||||
| | Audible Ringing Tone | |||||||||||
| How to get this software | ||||||||||||
| This example application is included as part of the CodeWarrior Development Studio for 56800/E Digital | ||||||||||||
| Signal Controllers. Follow these steps: | ||||||||||||
| 1. | Install CodeWarrior Development Studio for 56800/E Digital Signal Controllers | |||||||||||
| 2. | Launch CodeWarrior, and create new Processor Expert project | |||||||||||
| a. | Select File > New menu | |||||||||||
| b. | Select Processor Expert Examples Stationery | |||||||||||
| c. | Type project name | |||||||||||
| d. | Click OK | |||||||||||
| e. | Select DemoApplications > Telephony > CTG > 56f827 | |||||||||||
| f. | Click OK | |||||||||||
| 3. | Generate application code by selecting Processor Expert > Generate Code menu | |||||||||||
| Detailed documentation | ||||||||||||
| Documentation for this application is included as part of this example project. Expand Doc folder located | ||||||||||||
| in the project window by clicking on the + icon next to the folder, and open desired file by double clicking it. | ||||||||||||
| Freescale and the Freescale logo are trademarks of Freescale Semiconductor, Inc. All other product | ||||||||||||
| or service names are the property of their respective owners. | ||||||||||||
| ©2005, Freescale Semiconductor, Inc | ||||||||||||