MC68060 Software Package v. P1.00
(MAC Download)

This entry contains a downloadable version of the MC68060 Software Package for the MacIntosh.


This is Production Release (P1.00) of the 060 Software Package, packaged for use on a Macintosh operating system platform.

Release P1_00 fixes some problems found in release B2. Problems fixed are detailed in file "CHANGES" for rev_hist. P1 -- To retrieve the files which make up the package, simply double click on the icon, and tell the self-extracting software where to put the files.

Delete the self-extracting archive if you are short on disk space. This archive was made using the Stuffit Deluxe utility package under license from Aladdin.

Please READ the readme file in the package and all the *.doc files.

Please note that the source code is provided for reference only. We have no source code assembly-to-assembly conversion packages, and have no plans to (acquire/write/make available) any of these.