﻿/*
*         Copyright (c), NXP Semiconductors Bangalore / India
*
*                     (C)NXP Semiconductors
*       All rights are reserved. Reproduction in whole or in part is 
*      prohibited without the written consent of the copyright owner.
*  NXP reserves the right to make changes without notice at any time.
* NXP makes no warranty, expressed, implied or statutory, including but
* not limited to any implied warranty of merchantability or fitness for any
*particular purpose, or that the use will not infringe any third party patent,
* copyright or trademark. NXP must not be liable for any loss or damage
*                          arising from its use.
*/

/** \file
* Readme.txt for getting the first-hand knowledge of how to use the Example with NFC NXP Reader library.
* $Author: nxp62726 $
* $Revision: 1.0 $
* $Date: 2014-08-08 16:30:30 +0530 (Friday, 8th August 2014) $
*
*/
====================================================================================
Readme - Software for the CLEV663B v3.0 and PN5180 TFBGA64 performance board v1.0
====================================================================================

1. DOCUMENT PURPOSE:
	This document describes the steps to be followed to execute DownloadLib package as well as known problems 
	and restrictions.
2. DESCRIPTION:
	This example is an example to download firmware into 5180.

3. RESTRICTIONS
	a) The Software is restricted to list of supported NFC Reader Boards mentioned in point (10), connected to Contex M3 LPC1769 micro-controller from NXP. 
	   The APIs are intended for NXP contact-less reader ICs only, as such the APIs are not to be ported to any technology from any other vendor.
	b) NXP will not support porting to any other vendor platform. 
	C) To compile and flash this project into the controller, you need to import this project using NXP LPCXpresso v7.9.x.

4. LIST OF SUPPORTED NFC READER BOARDS:
	b) PN5180 TFBGA64 performance board v1.0