# Overview
 * 	-----------
 * 	The LPC845_BoB_CAPTocuh application shows how to interface with the on-board Cap touch button using SDK drivers.
 *  After an initial calibration, once the cap touch button is touched, the RGB red led will turn on.
 *
 *	## Toolchain Supported
 *	---------------------
 *	- MCUXpresso IDE v10.3
 *
 *	## Hardware Requirements
 *	------------------------
 *	- Micro USB cable
 *	- LPC845 Breakout board
 *	- Personal Computer
 *
 *  ## Board Settings
 *	------------------------
 *	No special settings are required. The project is set to output messages to the MCUXpresso IDE Console
 *