INTRODUCTION:
=============
This file contains the information related to the PN7642 FW specific files which are required for FW download related "C" array files
and default application certificates required for generation of the encrypted application fw for utilizing the encrypted fw download mode.


Files information:
==================



phDnldNfc_UpdateSeq_v02.05.c	==> Contains the "C" array equivalent of PN7642_v02.05.esfwu. 
									This file can be included as part of SDK exmaple application where NXP FW download is required from application on PN7642 IC.
phDnldNfc_UpdateSeq_v02.F5.c	==> Contains the "C" array equivalent of PN7642_v02.F5.esfwu. 
									This file can be included as part of SDK exmaple application where NXP FW download is required from application on PN7642 IC.
PN7642_Default_AESChipKey.txt	==> This is the default AES key provisioned @ KeyId=0x00 (128-bit), @KeyId=2,3 (256-bit). 
									This key is required to generate encrypted payload. 
									For the specific 12NC/9NC, please refer to the PN7642 datasheet to refer the key.
PN7642_Default_App_RSAKey.pem	==> This is the default RSA certificate installed in PN7642. The customer shall use this certificate to create a .esfwu 
									as mentioned in the instruction manual and rotate the RSA certificate to his/her own application certificate for further 
									encrypted FW download.
PN7642_SecureFW_SCR.pdf			==> SCR for PN7642 Secure FW.
PN7642_v02.05.esfwu				==> Encrypted FW for NXP region v02.05, this will also have default RF settings for 45x45 antenna.
PN7642_v02.F5.esfwu				==> Encrypted FW for NXP region v02.F5. This is same as that of v02.05, but the RF and protocol 
									settings are not overwritten.


=======END======